Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
M580 CPU firmware V2.90
Modicon PAC Forum
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-09-1703:54 PM
M580 CPU firmware V2.90
To clarify the question can I install the latest firmware on all M580 CPUs irrespective of the product version (PV) also known as the hardware revision.
The answer is yes the latest firmware can be installed on CPUs that have earlier versions of PV. The important note is that the latest hardware version as listed in the attached file, must use V2.90 or a later version of the firmware. It must not and cannot be downgraded to an earlier version.
The new CPU PV uses a newer internal switch when combined with the new firmware provides a more strengthened cyber security platform. V2.90 introduces a number of cyber security improvements it is not clear which of these are specific to the new PV and which apply to all PVs.