Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
M340 Real Time Clock Delay
Modicon PAC Forum
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-07-3012:55 PM
M340 Real Time Clock Delay
Hello Community,
I have a brand new PLC CPU M340 P342020, and I have a transfer program that I get from a Premium PLC. We have to make an upgrade from premiun to M340, but I'm having some issues with the real time clock, after I set the PLC Date and Time from the PC, after a couple of hours it beggans to delay some seconds from the PC Date and Time, It really concerns me because I need that the PLC to have the exact time because of the Generator Exercise, the whole reasone we are changing the Premiun to M340, is because also with the Premium we were getting the same trouble with the time, but as you all can se also with the M340 the time is no stay the same.
Is there a way that I can change some configuration or something to maintain the time in the PLC?