This is a more comprehensive package of links (Firmware link spreadsheet V4.1) than the one provided with SESU.
New update as at 2020-03-10
The attached spreadsheet lists collated links to publicly available firmware for M340/ M580/ X80/ Advantys/ Connexium.
Updated with:
- all embedded links point to se.com public sources
- X80 updates
Feedback welcome (broken links, improvements or additions needed).