Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Help transmiting data from M241 to modbus device
Modicon PAC Forum
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-03-0912:10 AM
Help transmiting data from M241 to modbus device
Hello guys,
I have created some structures in somachine in order to be transmitted with modbus from a M241 PLC. The problem is that all these data are being transmitted but not correctly. For example I have the following data:
W:int:=50;
VA:int:=1000;
Varpower:int:=2000;
Hz:udint:=50;
TotWhInj:ulint:=100;
TotWhAbs:ulint:=100;
So these data are being transmitted with modbus and I am checking with modbus poll whether the transmission is okay or not. So when I check on modbus poll I found out this:
- When I change the value of Hz (That occupy 2 modbus registers) it doesn't change the registers of Hz but change one register of Hz (The second one) and the first register of the next variable.
I am not sure why that is happening. But what I know is that If change the types from udint and ulint to uint everything works fine.
If someone could help me I would appreciate a lot. Thanks in advance!