Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80616members
346558posts

MODICON M221 EcoStruxure Weekly Timer

Sanzio94
Crewman
Crewman
0 Likes
2
640

MODICON M221 EcoStruxure Weekly Timer

Hello everyone, 

 

is there a way to program a weekly timer on EcoStruxure Machine Expert Basic that will give me a signal on set days and time?

For example I would want to be able to select through an HMI the day/s of the week and the time when the system will automatically start. I need the equivalent of a mechanical time switch in EcoStruxure. 

 

Thank you all in advance for your time. 

 

-Sanzio

 

 

Tags (1)
2 Replies 2
Bastian_Schmitz
Lt. Commander Lt. Commander
Lt. Commander

Re: MODICON M221 EcoStruxure Weekly Timer

Please have a look into the online help of ESME Basic.

Such a function is available

M22111.PNG

Attachments
Tags (3)
Sanzio94
Crewman
Crewman
0 Likes
0
515

Re: MODICON M221 EcoStruxure Weekly Timer

Thank you, really appreciated the help. 

 

-Sanzio

Tags (1)