Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80771members
346785posts

M340 M580 X80 firmware files V5.3

AlastairF
Lieutenant Lieutenant
Lieutenant

M340 M580 X80 firmware files V5.3

This is a more comprehensive package of links (Firmware link spreadsheet V5.3) than the one provided with SESU.

New update as at 2021-10-05

The attached spreadsheet lists collated links to publicly available firmware for M340/ M580/ X80/ Advantys/ Connexium/ Modicon switches.

Updated with:

  • M340
  • MC80
  • BMXAMI
  • BMXNOR
  • Advantys
  • EADM

Feedback welcome (broken links, improvements or additions needed).

 

Attachments
Tags (1)
1 Reply 1
Robert_Willis
Ensign Ensign
Ensign

Re: M340 M580 X80 firmware files V5.3

Thank you for your continued support at keeping this updated.

Tags (1)