Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80721members
346686posts

Learning Basic Program Modicon M221

PLCDROID
Ensign
Ensign
1
1338

Learning Basic Program Modicon M221

Tutorial Basic Program Modicon M221

 

This Tutorial Use Software EcoStruxure Machine Expert-Basic

 

List VIdeo: 

1. How to Instal EcoStruxure Machine Expert-Basic

 

2. How to Instal EcoStruxure Vijeo Designer Basic 

 

3. How to Import or Open Program EcoStruxure Machine Expert-Basic

 

4. How to Simulation EcoStruxure Machine Expert-Basic With HMI VIjeo Designer Basic

 

5. How to Configuration Hardware PLC Modicon M221

6. How to Create Function Timer 

 

7. How to Create Function Counter

 

8. Learning Program Arithmetic

 

9. How to make Program Running Light

 

10. How to Make Program 1 Tombol for ON and OFF

Belajar dan Belajar : www.plcdroid.com
Tags (3)
1 Reply 1
Maddison
Cadet
0 Likes
0
1272

i’m using the HMI5STU HMI and m221 PLC. Both are from Sch...

i’m using the HMI5STU HMI and m221 PLC. Both are from Schneider electric. I can’t seem to create a variable to change the PTO write parameter object. The end result i’m looking for is to create an input box on the hmi to control the speed and direction (constant velocity) of a closed loop stepper receiving pulse+dir inputs. If anyone has encountered the same problem, do leave a comment and hope some old timer can help us out. Thank you