Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80612members
346542posts

PM1000H LCD Modbus Data Sheet

yazeed_eastjo_c
Lieutenant
Lieutenant

PM1000H LCD Modbus Data Sheet

I need the modbus table to read the PM1000H LCD power meter values such as voltages, current, power factor, ...etc

Tags (1)
2 Replies 2
Satender
Cadet
0 Likes
0
89

Re: PM1000H LCD Modbus Data Sheet

Tags (1)
Charles_Murison
Picard Picard
Picard
0 Likes
0
239

Re: PM1000H LCD Modbus Data Sheet

Hello @yazeed_eastjo_c ,

 

If you are referring to the EasyLogicTM PM1000 Series Power Meter, please refer to the user guide, https://www.se.com/ww/en/download/document/NHA1696401/

 

In this guide the PM1200 meter supports Modbus RTU, the PM1000 does not. (page 13)

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)