Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Hi
I would like to prescribe both ION7650 + PME for its disturbance detection feature. Anyone has designed a page in PME for this feature?
Thanks
Abon
I have done this with the CM4'S with great success. What are you trying to do. 8 may be able to point you in a direction (may not be right or wrong but it will be in a direction).
Edit: Sorry I had to wait until I got to my computer to post the image. The arrow reflects the direction of the disturbance.
Can you post a screen shot?
To get the image to work based on value I had to modify the Schneider drivers "HIGHLY NOT RECOMMENDED". I planning on contacting to suggest a permanent driver modification. I also understand this could be done in the VIP, but that just adds CPU loading. I can walk you through the solution if you would like but don't want to put it up here as it is a change to drivers (for the CM4 it was a modification of about 6 lines in 2 drivers).
Definitely keen to see - send me a PM and we'll see if we can set something up. I'm keen to show you a few new things too.
Hi ,
Any updates on this feature? This is a strong selling point that we would like to realize as soon as possible.
Thanks
User | Count |
---|---|
199 | |
43 | |
38 | |
29 | |
14 | |
12 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.