41315members
184301posts

New front views for PIX Easy FR and PIX Easy MR are available in Ecostruxure Power Build MV

Highlighted
Ensign

New front views for PIX Easy FR and PIX Easy MR are available in Ecostruxure Power Build MV

Panel builders can use the layouts of the Primary Air Insulated switchgears PIX Easy FR and PIX Easy MR with new front views. The layout of the different cubicles in a project are now assembled to create a real and global layout of the project. 

In addition, projects are automatically archived after 30 days without any changes. You can decide yourself to archive or unarchive a project.

Olga - Business Owner Partners Software
1 REPLY 1
Highlighted
Administrator

Re: New front views for PIX Easy FR and PIX Easy MR are available in Ecostruxure Power Build MV

Hello Olga,

 

Thank you for sharing this useful information with the community. 🙂

 

Have a nice day.

 

Best regards,
Nedjma
Community Manager of Exchange Community