43549members
218144posts

Is it posible to create a personal library of cubicles in Ecoreal MV ?

Crewman
Crewman

Is it posible to create a personal library of cubicles in Ecoreal MV ?

I want to create my own library of  cubicles in Ecoreal MV, how can I do ?

2 REPLIES 2
Highlighted
Ensign

Re: Is it posible to create a personal library of cubicles in Ecoreal MV ?

Yes, when you enter in ESX Power Build MV, you get access to 3 menus : “My Projects” , “Archived Projects” and “My Settings”

clipboard_image_0.jpeg

Then, enter in “My Settings” and click on “Customized cubicles”. This will allow you to create a typical cubicle with the level of configuration that you wish.

clipboard_image_1.jpeg

This cubicle already preconfigured will appear in the list of the functional units accessible in the “Configure” menu of the software, ready to use for starting to build the SLD, single line diagram.

clipboard_image_2.jpeg

This functionality will help you to save time when you have recurrent cubicles in your daily business.

Highlighted
Crewman
Crewman

Re: Is it posible to create a personal library of cubicles in Ecoreal MV ?

Very usefull @BrunoPSDCX ,

thanks for your answer with the screenshots !