Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79357members
344053posts

Purge Connections for 80 GHz Radar

Jeff_Blair
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Purge Connections for 80 GHz Radar

If you decide to use a purge option with your 80 GHz radar, here is what it looks like. The purge option is available on these antennas and process connections:

  • Lens, DN40 (1-1/2”) with 1-1/2” threaded connections
  • Lens, DN70 (2-3/4”) with 3” threaded connections

It comes with a G 1/4 threaded connection on the air hose connection.

What's interesting is that the purge connection merely becomes an extension of your existing process connection.

 

Remember that a radar sees through dust.  But if you have an application where you think the build up will be so severe that it may cake and/or crust up very thick on the antenna, then a purge may be a good option and save some maintenance time.

 

Purging Connection.PNG

 

Tags (1)