42319members
209667posts

What we can learn from Google regarding radar level

Highlighted
Lieutenant JG

What we can learn from Google regarding radar level

Try typing this in google

"radar level transmitter for"

I think these are the topics that our customers want to learn about.

My plan is to make some collateral around the first four of these topics.

What else to we need?

 

 

2 REPLIES 2
Highlighted
Ensign

Re: What we can learn from Google regarding radar level

I would suggest some documentation explain why selecting 24GHz (K band) or 80 GHz (W band). For Example: Why using a LR74 or LR75? 

How may I help with Instrumentation?
Lieutenant JG

Re: What we can learn from Google regarding radar level

Great idea.  Thanks.