43549members
218144posts

Emerson AMS Device Manager Compatible Radar Level and Buoyancy

Highlighted
Lieutenant

Emerson AMS Device Manager Compatible Radar Level and Buoyancy

As we have customers in the field using the AMS product to manage their instrumentation systems, I wanted to volunteer the following information.

 

LG01 is a guided wave liquids and solids level radar compliant with AMS Device Manager

LR01 is a free space liquids level radar compliant with AMS Device Manager.

For driver information per our friends at Emerson: "Schneider Electric LG01 Guided Wave Radar and LR01 Free Space Radar are already integrated in AMS v14.0 and any newer version of the software as indicated in the Supported Device List of its Installation Media."

 

LR54 is a free space liquids level radar compliant with AMS Device Manager.

LR64 is a free space solids level radar compliant with AMS Device Manager.

LR74 is a free space liquids level radar compliant with AMS Device Manager.

LR65 is a free space solids level radar compliant with AMS Device Manager.

LR75 is a free space liquids level radar compliant with AMS Device Manager.

For driver information for LR54, LR64, LR65, LR74, and LR75, please download the DD file here:

https://schneider-electric.app.box.com/s/62qrqz7qlpjbizdlf10998ux5m95g34p

 

AMS does have flexibility to use our DTMs if desired:

Referencing https://www.emerson.com/documents/automation/brochure-device-list-ams-en-38408.pdf
" DTMs can be used with AMS Device Manager if the necessary functionality for a device is not found
in the DD. Please contact the device manufacturer to determine if a DTM is available for a given device.

 

Our radar DTMs can all be found for download at:
https://schneider-electric.app.box.com/s/hrhacpthoc4cq31rz7v34kiyivq0p6b9 (search for keyword "Software")

 

244LD is an Intelligent Buoyancy Transmitter for Level, Interface and Density.  

DDs and DTMs can be downloaded at:
https://schneider-electric.app.box.com/s/hrhacpthoc4cq31rz7v34kiyivq0p6b9 (search for keyword "Software")