Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79290members
343965posts

Is Revit MEP required to use LayoutFAST?

Solved
BIMtastic
Crewman
Crewman
0 Likes
1
502

Is Revit MEP required to use LayoutFAST?

Hello, I'm wondering if I need Revit MEP to use LayoutFAST.  I would prefer not to upgrade at the moment.  Thanks for the help.


Accepted Solutions
FelixRamos
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
499

Re: Is Revit MEP required to use LayoutFAST?

Hello, yes, Revit MEP (Mechanical, Electrical and Plumbing) is required. It should be noted, Revit Architecture and Revit MEP were combined in 2017.  Thanks for posting in our forum!

See Answer In Context

1 Reply 1
FelixRamos
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
500

Re: Is Revit MEP required to use LayoutFAST?

Hello, yes, Revit MEP (Mechanical, Electrical and Plumbing) is required. It should be noted, Revit Architecture and Revit MEP were combined in 2017.  Thanks for posting in our forum!