Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now

By Clicking on "Register Now", you acknowledge that you have read the Privacy Notice for Schneider Electric Exchange.

Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Will the I/A Series proprietary drivers work on a JACE-600 or JACE-700?

Issue

Will the JACE-600 or JACE-700 work with any of the four I/A Series proprietary drivers (GCM, DMS, ASD, MS)?

Environment

Niagara G3

JACE-600

JACE-700

Cause

Existing building retrofit

Resolution

The four proprietary drivers are not supported on the JACE-600 or JACE-700 controllers. If these drivers are required a JACE 645 (TRD-T-645) is required. Please refer to Product Announcement PA-00251 for further details.

Tags (2)
Labels (1)
No ratings
Contributors