Issue
Will VisiSat work with Windows Vista?
Environment
- VisiSat
- Windows Vista
Cause
Compatibility with Microsoft OS
Resolution
VisiSat Version 2.1 build 148 service pack 1 can either be used on a computer running Windows XP Pro with Visio 2003 or it can be used on a computer running Windows Vista with Visio 2007.
As detailed in the VisiSat 2.1 Configuration Tool Datasheet, available via Exchange OnLine, where you will also find the Installation/User's guide and the VisiSat Engineering Guides.
VisiSat Version 2.1 Build 148 service pack 1 is available for download via Exchange OnLine.
Note: File size = 41.5 Mb.