Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Where is SQL Service Manager in SQL 2005 and SQL 2008?

Issue

Setting up a single user (SQLExpress 2005) v1.93 CyberStation and the SQL Service Manager is not popping up like it should (on the Windows taskbar).

Environment

Standalone CyberStation

SQLExpress 2005

Cause

Previous versions of CyberStation had a SQL Service Manager application in the Windows taskbar. When installing a standalone v1.93 CyberStation this application is not there.

Resolution

SQLExpress 2005 does not install that application. This application is not required to run CyberStation.  If for some reason there is a need to stop SQL Server there is a workaround. Go to Control Panel>>Administrative Tools>>Services. Then scroll down to SQL Server (SQLExpress). You can stop SQLExpress by right-clicking it.

 



 

Tags (1)
Labels (1)
No ratings
Contributors