Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find current documentation for the WorkPlace Tech Tool software and the controllers that can be programmed using that software?

Issue

Where can I find the current documentation for the WorkPlace Tech Tool software, MNL LON controllers, MNB BACnet controllers and their associated specification data sheets.

Environment

WorkPlace Tech Tool software

I/A Series MNB BACnet family of controllers

I/A Series MNL LON family of controllers

Cause

There is no single online source for the all the current documentation for the WorkPlace Tech Tool software, MNL LON controllers, MNB BACnet controllers and their associated specification data sheets.

Resolution

All documentation related to the WorkPlace Tech Tool (WPT, WPCT & WPFB) and related controller documents are installed to your computer when you install the WorkPlace Tech Tool software. At the time of release, the current version of each software manual, hardware installation manual (LON & BACnet), specification data sheet (LON, BACnet & Software) and the software release notes document is built into the software installation program.

These documents are all accessible under the \WorkPlace Tech\Help folder on any computer where the WorkPlace Tech Tool software is installed. All documentation can be displayed from the list displayed by the WorkPlace Tech Help menu. This was done to insure that all WorkPlace Tech Tool users would have access to the version of all documents related to that specific release of the software.

Since these documents are included in the installation package for any version of the WorkPlace Tech Tool software, you can download the latest WorkPlace Tech Tool installation file from The Exchange Download Center to get the complete set of documents.
These documents are also available individually from the 'Publication Zone', accessible from the 'Links' menu on iPortal (https://iportal2.schneider-electric.com).

Tags (1)
Labels (1)
No ratings
Contributors