Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now

By Clicking on "Register Now", you acknowledge that you have read the Privacy Notice for Schneider Electric Exchange.

Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

When tunnel through a UNC using an HTTP port other than 80 the Ax Serial Tunnel will not connect and locks up.

Issue

When tunnel through a UNC using an HTTP port other than 80 the Ax Serial Tunnel will not connect and locks up.

Environment

R2, G3 I/A Series tunneling

Cause

Including the port number after the IP address when entering the Host address in the Ax serial tunnel window will cause it to lock up trying to connect with the port entered.

Resolution

Do not include the port number after the IP address when entering the Host address in the Ax serial tunnel window.

Tags (1)
Labels (1)
No ratings