Issue
New computer hardware was provided for SIGNAL. The SIGNAL folder from the previous hard drive was copied and pasted to the new computer's hard drive.
When SIGNAL is started, a pop-up error message appears:
User Build error, Btrieve # 910 INI path error
Environment
SIGNAL all versions
Cause
New computer hardware provided and the original floppy diskettes are not available.
Resolution
The following two things cause this error:
- Windows User Account must have administrative privileges
- the \windows folder must have the bti.ini and signal.ini files