Issue
When accessing an SNP network with SE Vista values are not displayed.
Environment
UK
Cause
SE Vista does not support 0 as a LAN number
Resolution
- Edit the XBuilder exported file to change the LAN number from 0 to 1.
- The XMLM file can be opened with Windows notepad.exe
-
Change "
To"