New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

What type of remote/external sensor can be connected to a SE7000 series thermostat?

Issue

Installing a SE7652A5045P and want to add an outside air and supply air temperature sensor.  What type of sensor is accepted?

Environment

SE7000 series room controllers

Cause

Spec requirement

Resolution

The SE7000 series sensor can take any 10k ohm NTC thermistor (type 2).

For a temperature / resistance chart, see page 6 in this guide.

For a Schneider-Electric compatible sensor, see page 7.

Tags (158)
Labels (1)
0% helpful (0/1)