Issue
What is the part number for the thermowell for the sensor TT-I-6-1?
Environment
TT-I-6-1
Cause
Replacing the thermowell for sensor TT-I-6-1.
Resolution
The thermowell for sensor TT-I-6-1 is either W-S-6-1/2-1 for 1/2" mpt and 6" long well OR W-S-6-3/4-1 which is for 3/4" mpt and 6" long well.