Issue
What is the operating temperature / humidity of Continuum controllers
Environment
Continuum
B3xxx
i2xxx
IO module
ACX52xx
ACX54xx
CX9xxx
Cause
The operating Environment for the Continuum controller range
Resolution
The operating Environment for the Continuum controller range is as follows:
Temperature
32°-120°F (0-49°C)
Humidity
10-95% RH (non-condensing)
This is the maximum Temperature and Humidity within the controller(s) enclosure, if the room is at 49°C then the temperature within the enclosure may be much warmer.