Issue
What is the Thermowell part number for the sensor TT-I-4-1?
Environment
TT-I-4-1
Cause
Replacing the Thermowell for sensor TT-I-4-1
Resolution
The thermowell for sensor TT-I-4-1 is either the W-S-4-1/2-1 for 1/2" MPT 4" long well or W-S-3/4-4-1 for 3/4" MPT and 4" long well