Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

What gender are the DB-25 connectors on the DM-20, DIO-20 and DO-20?

Issue

Need to know the connector genders to order the interconnecting ribbon cable.

Environment

DO-20 DM-20 DIO-20

Cause

Not in the documentation for the DO-20.

Resolution

All three have a female DB25 connector. Also, the interconnecting cable from the DM-20 to the DO-20 or DIO-20 is a straight-through 25 conductor cable.

Tags (1)
Labels (1)
No ratings