Issue
Question on what to set the virtual memory to on a Continuum Workstation PC
Product Line
Andover Continuum
Environment
Windows XP
Cause
Question on what to set the virtual memory to on a Continuum Workstation PC
Resolution
Virtual Memory Requirements
The virtual memory "Initial size (MB)" setting on your workstation PC should be set to a minimum of 1 GB. To make this change:
- Go to Start, Settings, Control Panel.
- In the Control Panel, double click System. The System Properties menu, shown on the next page, appears.
- Click the Advanced tab and click Settings in the Performance box. The Performance Options menu appears.
- Click the Advanced tab. In the Virtual Memory box, click on Change. When the Virtual Memory dialog appears, fill in the desired paging file memory size (initial and Maximum).
- Click OK as you back out of the dialogs.