Issue
What components make up the LON-TERM1 and LON-TERM2 terminators?
Environment
- LON-TERM1 terminator
- LON-TERM2 terminator
Cause
LON-TERM1 and LON-TERM2 terminators are required for MicroNet LonWorks network topologies.
Resolution
The LON-TERM1 uses a capacitor in series with a resistor with each part having the following specs:
- Resistor E19-607 52.3 ohms, +\- 1%, 1W, MF
- Capacitor E13-468 47 uF, +\- 20%, 50WVDC, Elec
The LON-TERM2 uses a capacitor in series with a resistor with each part having the following specs:
- Resistor E19-608 105 ohms, +\- 1%, 1W, MF
- Capacitor E13-468 47 uF, +\- 20%, 50WVDC, Elec