Issue
What command displays the translation of the IP addresses to Ethernet addresses?
Environment
I/NET
Cause
This stands for Address Resolution Protocol (ARP). This command displays the table of translations between IP addresses and Ethernet Addresses. This table is built dynamically. When ARP receives a request to translate an IP address, it checks for the address in the (ARP) table.
Resolution
arp -a