Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

What camera conditions does Continuum support being shown as a Continuum alarm?

Issue

What camera conditions does Continuum support being shown as a Continuum alarm?

Environment

Continuum v2.0

Pelco Video Server

Digital Sentry

Endura

Cause

Available documentation is a bit bare on specifically what camera conditions can be monitored / setup to be displayed as alarms in Continuum.

Resolution

According to the Video compatibility matrix:According to the Video compatibility matrix: Only the following video alarms are supported:
According to the latest Video Compatibility Matrix, the following video alarms are supported:
  1. video server online/offline
  2. camera video loss (cable connection loss only, not covering of camera lens)
  3. motion detection (per camera)
 
Note: Video loss and motion alarm functionality not supported on DVX and DVXi Video Servers.
 
1) video server online/offline, 2) camera video loss, and 3) motion detection (per camera).
 
DVX and DVXi do not support video loss and motion alarm functionality.
 
QA indicates we do support video loss (cable connection loss only) but not when the camera is covered
 
So we do support Video Loss and this looks to be per camera as another Engineer noted his system showed specific camera names in the video loss alarms showing in Continuum. This would be video loss from cable disconnect not from a camera lens being covered though.
 
new Compatibility Matrix for Video as well. Just released.
Tags (1)
Labels (2)
No ratings