Issue
- Font size is very large in Xenta Server and Webstation TGMLs, both in the web interface and when viewing from Vista
- Text in TGML graphics is too large, it word wraps when it shouldn't
Environment
- TAC Xenta 700
- TAC Xenta 511
- TAC Xenta 527
- TAC Xenta 555
- TAC Vista
- TAC Vista Webstation
Cause
Windows Font Size is set to more than 100%. It has been found set to 125% as default on some PCs.
Resolution
In Windows 7 and 2008 Server:
- Goto Control Panel -> Appearance --> Display
- Click "Smaller - 100%" option and then apply settings
- The font in TGMLs should now display normally