Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Webclient unavailable DCOM error or webclient is currently unavailable

Issue

Webclient currently unavailable Error 80070005 Check your DCOM permissions when launching webclient or webclient is currently unavailable.

Product Line

Andover Continuum

Environment

  • Webclient
  • Windows XP
  • Windows 7
  • Windows Server 2003
  • Windows Server 2008

Cause

A remote reboot will not write DCOM permissions the same way a local reboot does. Other Server configurations can cause this.

Resolution

  1. A webClient installation was performed using Windows Remote Desktop or some other remote access software and the reboot after the webclient install was executed using the remote software.
    To fix this, reboot the Webclient server directly from the server itself. There are security permissions that do not get written properly when rebooting remotely and a direct reboot corrects this problem.
  2. Start Continuum on the Webclient PC locally, not remotely. Be sure Continuum has been started on the webclient PC.
  3. Also see, Webclient unavailable error when attempting to logon which mentions making sure the Network Service is selected for the default app pool.
  4. 64-bit OS will cause this error as well. Webclient versions pre 1.94 are not supported on any 64 bit platform.
  5. If that doesn't work then a complete reinstall and reboot on the server will be required. Remote installs are typically problematic.
  6. If changes were made to .net try the following steps:
  • Start> Run> cmd (Enter)  To get to a DOS prompt
  • cd\Windows\microsoft.net\framework\v2.0.50727 (change directory to this folder)
  • run the command aspnet_regiis.exe -i (It will say installing .net, this re-registers .net with IIS)
  • Restart Windows on the webclient PC and restart Continuum
Tags (9)
Labels (1)
No ratings