Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Webclient "There was an error trying to create the .NET control for this page"

Issue

A dialog of "Cannot open .NET editor with .NET Framework" comes up with new installation of Webclient or after a Microsoft update of .NET 4.5.x.

webclientScheduleNetControl.jpgThere was an error trying to create the .NET control for this page.

Product Line

Andover Continuum

Environment

  • Windows 7
  • Windows Server 2008
  • Internet Explorer

Cause

Microsoft changed the behavior of Internet Explorer when .net 4.5.x is installed on a PC. It turns off .net 2.0 support which is needed for several editors to function on Webclient browser PCs

Resolution

See web.Client v2.0 .Net Editor Hotfix on the Download Center. This is a registry key file that installs the registry keys mentioned further down in this article. It allows Internet Explorer to utilize .net 2.0 that several webclient editors use.

This hotfix contains a .reg file which changes the registry, it is recommended to make a Windows Restore point or a backup (export) of the existing registry folder (hive).

The hotfix only updates the following keys

  1. On an x86 Operating System
    1. Add a DWORD attribute with the name EnableIEHosting to KEY_LOCAL_MACHINE\SOFTWARE\Microsoft\.NETFramework
    2. Set the value to 1
  2. On an x64 Operating System
    1. Add a DWORD attribute with the name EnableIEHosting to KEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Microsoft\.NETFramework
    2. Set the value to 1

A reboot of the webclient browser PC is required after the change is made. Each browser PC will need to have this fix applied.

For more information see Microsoft's Application Compatibility in the .NET Framework.

Tags (3)
Labels (1)
No ratings