New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Announcements

- Discover the Exchange Community Top members of October here!

- The member of the month: Vassil, EcoXpert Master read the article here!

Webclient Pre-Installation Requirements for Windows Server 2016

Issue

WebClient Pre-Installation Requirements for Server 2016 are not included in the 2.03 webClient installation guide

Product Line

Andover Continuum

Environment

  • Windows Server 2016
  • Continuum webClient Server 2.03

Cause

The Pre-Installation requirement steps provided in the webClient planning and installation guide do not show all the steps needed to install webClient successfully

Resolution

This material is intended as a supplement to the webClient Planning and Installation Guide

 

Installing IIS on Windows Server 2016
For Windows Server 2016, install IIS on the designated web.Client application
server (LAN systems) or the standalone CyberStation/web.Client workstation
(standalone system).
1. Start the Server Manager by clicking on the Administrative Tools menu.
2. In the Server Manager, click Add Roles and Features.
3. In the Add Roles and Features Wizard, Before You Begin tab, click Next.
4. In Installation Type, select Role-based or feature-based installation.

Select Installation TypeMan.png

5. Click Next and then select a server or virtual hard disk on which to install
roles and features.
6. In Server Selection, click Select a server from the server pool.

Server Selction Man.png

7. Click Next and select one or more roles to install on the selected server.
8. In Select Server Roles, please select the items from the following snapshots carefully

Note: In previous Windows Server instructions from the webClient pre-installation guide, a reference was made to select Application Server. This option is selected and installed by default in Windows Server 2016.

No selection for Application Server is offered.

 

Select Server Roles1.png

Select Server Roles2.png

Select Server Roles3.png

Select Server Roles4.png

Select Server Roles5.png

Select Server Roles6.png

Select Server Roles7.png

Select Server Roles8.png

Once these Pre-Installation steps have been performed the webClient Server is ready for Chapter 4 - Installing web.client on the IIS PC (Found in the webClient planning and installation guide.pdf)

Tags (1)
Labels (1)
No ratings
Contributors