Issue
Does TAC Vistas new OPC server (version 1.1.0) that was released with TAC Vista 5.1 only work with Vista 5.1?
Environment
- Vista 5.0
- OPC server 1.1.0
Cause
Because the new version of OPC comes with Vista 5.1, it may be assumed that it is not fully backwards compatible.
Resolution
OPC server version 1.1.0 is compatible with all Vista 5 versions.