Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Veris HW sensor part number for displaying both the temperature and humidity readings on the sensor's LCD

Issue

Veris HW sensor part number for displaying both the temperature and humidity readings on the sensor's LCD

Environment

Veris HW Series deluxe wall humidity sensors

Cause

There is a need to display both the humidity and temperature readings on the sensor's LCD

Resolution

In order for unit to display both temperature and humidity, use the TA or D temp selection in the part number.

Refer to the HW series sensors datasheet.

Tags (1)
Labels (1)
No ratings