Issue
Are the current Veeder Root Xdrivers compatible with the TLS450 and TLS2P console?
Environment
Xdriver
Cause
The current Xdrivers are compatible with the Veeder-Root TLS350 Console. Are the current Veeder-Root Xdrivers compatible with the TLS450 and TLS2P console?
Resolution
No. The current 1st and 2nd Generation Continuum compatible xDriver for Veeder-Root TSL300/350/350R is not compatible with the TLS450 or TLS2P. For the current Xdriver see
Leak Detection Systems Drivers on The Exchange Download Center.