Issue
Engineer is using his I/A Series R2 notebook to edit customer's UNC station.
Getting errors in Standard Output Window regarding out of data modules and missing modules.
Environment
I/A Series R2 WPP and UNC.
Cause
Engineer's copy of WPP does not have the same version of the I/A Series R2 software or some of the modules are not of the same revision. UNC station was originally edited from the Enterprise Server on the site.
Resolution
- Insure the version of all modules used in the UNC match those installed in the nre\modules folder of the WPP system.
- Insure that the version of the NiagaraD service being run on the computer matches the version of software installed in the UNC.