Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Value of an I/NET DO Point does not stay after Manual Control in Vista

Issue

When controlling I/NET DO point in Vista, for example changing the value from "0" to "1", the value of the point won't stay. It changes back to "0".

Environment

I/NET integrated to Vista (I2V)

Cause

There are several attributes of an I/NET DO point (shown below in Vista). Usually the "control" attribute is used to manually control the DO point, while "value" is used to monitor the current state of the DO. If the "control" attribute is changed from "0" to "1", the real DO point will be on, but value of this "control" property point will change back to "0".

Resolution

Use the "control" attribute to manually control the DO point. Use the "value" attribute to monitor the current state of the DO point.

Tags (3)
Labels (2)
No ratings