Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Using Sysman Alert Server with EcoStruxure Building Operation

Issue

Is it possible to use Sysman Alert Server with EcoStruxure Building Operation?

Product Line

EcoStruxure Building Operation

Environment

Alarms and Events

Cause

Customers may wish to send important alarms to duty staff via SMS. Sysman Alert Server is one way of doing this and is easy to configure. 

Resolution

This is possible. The following document details the setup procedure: Sysman Alert Server with StruxureWare Building Operation

The configuration will depend on the setup and location of the SysMan Server, but will generally involve "Write to File" Notifications if the Enterprise Server and Sysman Servers are installed on the same PC, or Emails to the SysMan Server (from Enterprise or Automation Server)

More information can be found on Sysman's website.

Part Numbers:

  1. SysManSMS ALERT SERVER: 900800600
  2. SysManSMS GSM Modem: 900800610

In the UK when ordering please use the below part numbers.

  1. SysManSMS ALERT SERVER: 802000
  2. SysManSMS GSM Modem: 100002
Tags (6)
Labels (1)
No ratings