Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Under objects such as Doors and Inputs what is the "Commands" option used for?

Issue

Under objects such as Doors and Inputs what is the "Commands" option used for?

Product Line

Security Expert

Environment

Security Expert

Cause

Unsure how to use the Commands option showing in some of the objects options.

Resolution

These cannot be adapted for general use by installers/integrators. These are mostly used for controller instructions that have been included in the firmware but have not been built into the UI yet, as well as internal testing. Leave these alone unless you have a specific need and the instructions from Product Support on how to configure the command.

Tags (1)
Labels (1)
No ratings