Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to set the nciSpaceTempOfst to a negative number in the Xenta 104-A plug-in

Issue

The Xenta 104-A plug-in limits the temperature value input between 0°F and 18°F. It is not possible to input a negative value.

Environment

Xenta 104-A Plug-In

Lonmaker 3.1 or Lonmaker 3.2

NL220

Cause

The Xenta 104-A plug-in limits the temperature value input between 0°F and 18°F. It is not possible to input a negative value.

Resolution

In Vista follow these steps:

  1. Navigate to the Xenta 104-A controller.
  2. Browse down to the Node Object function block and find the nciSpaceTempOfst SCPT.
  3. Type in the designed space temp offset parameter from the default 32°F value.

For example, if a -1°F offset is needed a value of 31 will need to be entered. If a +1°F offset is needed a 33 will need to be entered. 32°F represents zero offset.

Tags (3)
Labels (1)
No ratings