Issue
I'm looking for a part number for the ATV 21 Variable Speed Drive but it does not appear on the part number list
Environment
ATV 21
ATV 212
Altivar
Variable Speed Drive
Cause
Part number has been discontinued
Resolution
There is now a new name for the ATV 21 Variable Speed Drive as this old version has now been updated
The new name for the ATV 21 is ATV 212 or Altivar 212
the below is a link to the Schneider Electric web site where all documentation, part numbers, distributors and Support can be found