Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to access the "Tools" menu item to configure options in the "standalone" version of I/A Series G3 Alarm Portal

Issue

Unable to access the "Tools" menu item to configure options in the "standalone" version of I/A Series G3 Alarm Portal

Environment

I/A Series G3, Alarm Portal, ENS-ALM-CON-G3

Cause

The "Tools" menu item was removed in I/A Series G3 versions 3.6 and higher to prevent any user from configuring Alarm Portal options (e.g. appearance and operational behavior).

Resolution

Configuration of the Alarm Portal options on a "standalone" version requires a set of files to be transferred from a full Workbench version of the Alarm Portal to the standalone version.

  • Start Workbench and select Tools - Options

  • Configure options (e.g. Alarm Console, Alarm Portal)

  • Close Workbench and use Windows Explorer to locate the options subfolder for the user that modified the Alarm Portal options

Copy the associated options files (alarm-AlarmConsoleOptions.options and alarm-AlarmPortalOptions.options) to the standalone Alarm Portal. Place the files under the appropriate user using the same path structure in an options subfolder.  The Alarm Portal will now use the options defined.

Tags (1)
Labels (1)
No ratings