Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

USB converters used with computer and interfaced equipment

Issue

My computer has USB ports, but it does not have serial or com ports. Can I use USB ports?

Environment

For I/NET, Host computer that either Direct Connects (cable 072) or you need to connect to a controller such as a 7798C (cable 082)

Continuum, Vista, Sigma, I/A Series, Pelco, DVR, DS, Com Port, Com, PTZ Control, Serial Port, Comm, Comm Port

Cause

USB to Com has issues downloading or communicating with system.

Resolution

The generic drivers which came with your USB to Com adapter do not allow two-way communication. 

Prolific driver often helps resolve this issue. Download driver HERE or for the latest driver use link below:

http://www.prolific.com.tw/US/CustomerLogin.aspx    you will need to logon as GUEST  

Tags (1)
No ratings