Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Tips to speed up saved searches in StruxureWare Building Operation

Issue

Tips to speed up saved searches in StruxureWare Building Operation

Product Line

EcoStruxure Building Operation

Environment

StruxureWare Workstation

Cause

Searches take a large set of objects and check them against text matching and then against conditions. The more you can eliminate before checking text or conditions the better.

Resolution

Whenever possible use the following methods to speed up searches

  • Use the 'In folder' field to avoid searching too large a section of the system
  • Do not include properties or sub-servers when they are not needed
  • Specify the smallest subset of type you are able to. For example, if you only want Extended Trend Logs, do not use the Base Trend Log object.
Tags (1)
Labels (1)
No ratings