Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

This NPR 2000 communicates fine on one network segment but not another

Issue

This NPR 2000 communicates fine on one network segment but not another. Why?

Environment

I/NET Site

Cause

This NPR 2000 communicates fine on one network segment but not another. Why?

Resolution

A site has the NPR 2000 which refused to communicate on the Ethernet. When they moved it from a 400 foot LAN segment to a 100 foot segment, it worked. Although 300ft. is the standard limit, the ferrite ring on the internal network jumper may have some impact on that. For that matter, if that jumper is suspect for any reason, the network cable can be plugged directly into the NPR 2000s NIC card temporarily for diagnostic purposes.

Tags (1)
Labels (1)
No ratings