Issue
Is the communications card in a UNC 126 the same as the NIU type 1?
Environment
UNC 126 outstation
NIU
Cause
Need to replace the communications card of the UNC 126 with an NIU type 1.
Resolution
Yes, the communications card of the UNC 126 outstation can be replaced using the communications card from an NIU type 1.