Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Telnet Port 23.

Issue

Port 23 is opened through Telnet and can provide a security access breach into a system.

Product Line

TAC INET

Environment

All versions of I/Net Software on All Supported Operating Systems.

Cause

When the Delta Debug tables are set to 1 or 2, it opens up port 23 for use but also Telnet can be used as well.

Resolution

The following steps need to be followed to resolve this issue:

  1. Go to Run and type regedit
  2. Open up HKEY_LOCAL_MACHINE
  3. Expand the Software tab and expand CSI-Control Systems International
    1. On x64 Based Systems the above folder is located under the HKEY_LOCAL_MACHINE\Software\WOW6432Node
  4. Open up the Configurations tab and click on the Active Configuration that is currently running in I/Net
  5. On the right side window, scroll down to Debug Tables, right-click and modify the setting
  6. Change the value to a 0, close out of it, close I/Net and I/o server and restart it again.

P.S. This should close that port but be aware that Telnet would not be able to function when this is done.

Tags (1)
Labels (1)
No ratings